Industry Online Support
Technical Forum
12/15/2014 8:03 AM | |
Posts: 84 Rating: (0) |
Hi all, I have two programs, and I want to take "AS" form one to the other, what is the correct procedures for that? Thanks
|
12/15/2014 2:47 PM | |
Posts: 84 Rating: (0) |
Thank you alot. I mean the second, but when I press right click, it give me the option of copy in grey colour, so I can't do it. regards
|
12/15/2014 3:08 PM | |
Posts: 32 Rating: (4) |
hmmm.... I'v tried it out and it worked fine here (see attachments). It also works when your CPU is running and you're working in some CFC or the HW Config is open. I'm not sure why you can't copy your station.... Are you sure you did a right-click on the station (component view) like in the attachments and not on the project ? Maybe you can show me a screenshot of your SIMATIC Manager? Regards
AttachmentCopy_AS_before_and_after.zip (85 Downloads) |
12/15/2014 3:28 PM | |
Posts: 84 Rating: (0) |
Accoding to your attached file, I want to copy the project "Teste_Prj", this is what I mean by 'AS'. Regards
|
12/15/2014 4:06 PM | |
Posts: 32 Rating: (4) |
Ok now I understand... Go for this: 1. If the project you want to copy is part of a multiproject, you have to remove the project from it (see attachment 1) 2. Open the preject and click "File > Archive..." (see attachment 2) 3. Retrieve the project to an other Folder (Maybe rename the folder afterwards) 4. Now you have the same project twice (see attachment 3) 5. Open the multiproject, rightclick on it and choose "Multiproject > Insert into Multiproject" (see attachment 4). 6. Select your project and repeat it with the second one. 7. Now you have "copied" the whole project (see attachment 5) Hope I could help you regards
AttachmentSteps.zip (80 Downloads) |
12/15/2014 4:22 PM | |
Posts: 84 Rating: (0) |
Thanks alot, it's OK but could you tell me about "Remove for editing"? when we use it? Regards
|
12/15/2014 4:37 PM | |
Posts: 32 Rating: (4) |
So that's from the manual PCS 7 Engineering Station (Link): Removing a Project from the Multiproject (Alternative) Note You can also move a project to a distributed engineering station as follows: 1. In the component view of the SIMATIC Manager select the project within the multiproject that you remove from the multiproject. 2. Select the menu command File > Multiproject > Remove for Editing... The "Select Directory" dialog box opens. 3. Select a directory and click "OK". Result The project is marked as "removed for editing" and displayed in gray. When a project has been removed, in contrast to the procedure described above, you can notuse the "Archive", "Save As", and "Compile OS" functions. For more information about "Remove for Editing..." see chapter 8.8.4 in the manual above. |
12/16/2014 10:39 AM | |
Posts: 84 Rating: (0) |
Thanks |
Follow us on