5/23/2019 1:25 AM | |
Posts: 24 Rating: (0) |
Hello,what if I want to point to an ARRAY in a DB with this function ? What I need to do is move the information that I have on the ARRAY to another DB but not in an ARRAY. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/23/2019 07:22:28New subject after splitting |
|
5/23/2019 8:15 AM | |
Posts: 2826 Rating: (684) |
Hello. This reply assumes you are using Step7 V5.x. The "blockmove" instruction is only concerned with the absolute address position. Ignore the fact that the data is structured. Only use the addressing markers. See the post that you linked from originally for an example, if you have doubts. Show us the structures and addresses of the data sets (screen capture pictures), if you require more guidance. BR |
Follow us on