1/28/2021 7:41 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, Simatic Shell is an application to configure the terminal bus and redundancy of your PC station. If you have a laptop with the PCS7 software installed, you can simulate your project by using PLCSim. PLCSim must be installed by the PCS7 media DVD and you need a license for it to use. Please note, that PLCSim lacks the use of named connections. You need to configure the connection for TCP/IP or ISO protocol. Please take not if you are using Route Control, you cannot use RC with PLCSim, since it requires a named connection. You can consult the following manual for more information (see chapter 12.1) : Engineering System V9.0 SP1 |
Last edited by: Jen_Moderator at: 01/28/2021 12:35:52Optimized link. If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on