Industry Online Support
Technical Forum
5/15/2013 9:40 PM | |
Joined: 10/3/2012 Last visit: 2/10/2022 Posts: 6 Rating: (0) |
Hi All, Have a problem with creating the script to open doc./pdf./xls. files using the"StartProgramm" function. Reading the manual (https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=51723931&caller=view&errcode=ERRCODE_CHANGEPASSWORD_OK) didn't help. The main problem is to correctly specify the Programm name and Programm parameter in the script: In the table from manual there is a programm name example kind like\windows\wt6explr.exe. The same problem how to correctly specify the path of programm parameter. From the example in manual it looks like\Storage Card SD\MachineData_01.doc(*.docx). But i need to open it from /d hardware in PC. Could you please explain what meanswindows\wt6explr.exe? Is some standart .exe which windows 7(64) uses to open files? Is it possible to provide some working scripts examples i can use to solve my problem? I use: Tia portal, WinCC V11, SP2. Would appreciate any help as this is quite a blocking for me at the moment. |
5/21/2013 11:51 AM | |
Posts: 3037 Rating: (192)
|
Hello, You create a message window for system messages. Which message appears im the message window if you click on the button? Tweety |
Follow us on