1/27/2009 5:37 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello You can't use the same way like old WinCC version. Some channels, which could be implemented with WinCC V5.1 until now, are no longer included with WinCC V6.2. WinCC has placed increased emphasis on communication via OPC. Information on how to establish a connection using the OPC communication driver is available in the WinCC Information System under the topic "Communication" and in Internet on the OPC Foundation homepage: http://www.opcfoundation.org/ (ForAllen Bradley DH DH+ DH485 recommendCyberlogic OPC Server regards |
Last edited by: UMENCHO at: 1/27/2009 5:38 PM |
|