3/9/2016 1:20 AM | |
Posts: 1 Rating: (0) |
Hi! There is an example in the manual: "
50 controllers are intended to be operated in a CPU315-2 PN/DP (6ES7315-2EH14-0AB0). If the OB3x cycle is 2 ms and one controller per OB3x cycle is processed, the resulting sampling time of controller is 100 ms. If two controllers are called per OB3x cycle, the sampling interval of the controller is halved to 50 ms (with higher OB1 load). " I want to ask how to realize that "one controller per OB3x cycle is processed" ? Is there any parametes for it? best regards
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/10/2016 2:45:20 PMNew subject after splitting |
|
Follow us on