6/1/2021 9:55 AM | |
Joined: 10/23/2018 Last visit: 11/10/2023 Posts: 6 Rating: (0) |
Hello, I have a problem with the process historian and I need to reset it. The version is 2014 SP2 The historian works fine, it does its reports all right. But I declared a new tag folder in the tagloggin and uploaded it to the historian, and it was uploaded but the graphs were not seen in the historian, no value (in trens in the runtime if the graphs were seen), I think it was because of the name "TES_Heat". Then I decided to delete it from the tagloggin, put the tags in SytemArchive and upload it again to the historian. But when I did it again, they were uploaded to the SystemArchive but the "TES_Heat" folder was not deleted. I was wondering if someone knows how to reset the historian so that it updates and leaves it as it is in the taglogging currently. Thank you very much. ------------------------------------------------------------------------------------------ |
Last edited by: xelatec at: 06/01/2021 09:55:24Last edited by: Jen_Moderator at: 06/01/2021 12:36:55New subject after splitting |
|
Follow us on