6/22/2017 1:48 PM | |
Joined: 12/2/2015 Last visit: 2/26/2024 Posts: 64 Rating: (7) |
Dear all, I know there is possibility to run oldest version panel in newer TIA. Proof for that is my situation: In project view (TIA v 13SP1) I have everything ok and I can simulate in RT old panel in version 11, but if I want only simulate version (as stand alone) from folder located on my hard drive in project directory \IM\HMI\{11866113-1738}\Generates\pdata.fwc there is a error: Anyone knows how run RTsimulation standalone for older version panels? ------------------------------------------------------------------------------------------ |
Last edited by: LuWiack at: 6/22/2017 1:49:20 PMLast edited by: Jen_Moderator at: 6/23/2017 2:21:18 PMNew subject after splitting |
|
6/23/2017 3:00 PM | |
Posts: 648 Rating: (95) |
LuWiack
Dear LuWiack, you can simulate older versions with the engineering system. The IM folder is the combiled RT project and can only open with the right version of WinCC RT Advanced. You need RT Advanced V11 or you make the simulation with your Engineering. Standalone is not possilbe. With best regards rh1990 |
6/30/2017 5:03 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Dear LuWiack, you startet the Runtime Advanced V11 so simulate the Runtime project of the Panel. But you need RT Advanced Version V13.0.1 because your choosen panel has the firmware V13.0.1 Install the "Advanced Simulation" from the DVD. You can start the simulation via the button left next to the runtime button. With best regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|