Industry Online Support
Technical Forum
10/29/2014 6:29 AM | |
Posts: 122 Rating: (1) |
Hello Experts, I am having tow offline projects but of with different version. Different version I meant that, one project is updated with latest changes and another with not. By using the block compare option I compared . Once on comparing if it shows the message that one path has latest version or newer version. I use to clik the GoTo option at the below of that pop up window. If I click it, it opens the tow different blocks but the blocks which was compared. But it does not highligt where the changes or difference is there between the tow. Neither I have an option in the menu to see the difference. Below that there is also a dash board where I could see some messages but it does not reveal where exactly the changes is. It would be nice if any option availbale to find the code differnce. Because right now I have to check for bunch of blocks the differences. But could not locate the difference. It would be nice if any one could tell if any options available to high light the changes in the code in Step 7 Graph. I here with attach you the snap shots. Looking forward to hear from you. With regards Johannes
AttachmentNeuer ZIP-komprimierter Ordner.zip (111 Downloads) |
10/29/2014 7:48 AM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, you can export the blocks as gr7-source and compare it e.g. with WinMerge. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools |
This contribution was helpful to1 thankful Users |
11/2/2014 7:02 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, in the block editor you can create source file and in the source folder you can export it. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools |
Follow us on