5/20/2020 10:17 PM | |
Posts: 6 Rating: (0) |
Hello! I am new to logo and am trying to set any parameter T programatically for many delay blocks at once. Ideally I want to be able to set the parameter through a network connection (by reading one of the local variable memory VM slots). The help says: > The actual value of another already-programmed function can provide the time in parameter T Then follows a list of analog blocks and the counter. I could not get any of these to work. The only thing that did work was a workaround like this: The error message that it shows in the status bar is: "Recursions only allowed via outputs and flags" Is this a bug in Logo Soft? I am using the Demo: V8.0.0.0 Thank you! Attachmentwatering.zip (137 Downloads) |
Last edited by: whnr at: 05/20/2020 22:34:04 |
|
5/20/2020 10:22 PM | |
Joined: 12/18/2014 Last visit: 5/8/2024 Posts: 32991 Rating: (4076)
|
Hello whnr, at first welcome to the forum. Please upload your program as a zip file. |
5/20/2020 10:34 PM | |
Posts: 6 Rating: (0) |
Thank you! I attached it to the original post. |
5/20/2020 10:52 PM | |
Joined: 12/18/2014 Last visit: 5/8/2024 Posts: 32991 Rating: (4076)
|
Something like this? |
This contribution was helpful to1 thankful Users |
5/21/2020 5:42 AM | |
Joined: 12/18/2014 Last visit: 5/8/2024 Posts: 32991 Rating: (4076)
|
Hello whnr, you're welcome ... |
Follow us on