2/18/2015 8:40 AM | |
Posts: 3 Rating: (0) |
dear ser, i want modify feedback dc motor from tacho generator to encoder spesification of dc motor 520 kw, 800 vdc, 700 amp and 1200 rpm spesification of tacho 100v/1000 rpm and spesification of encoder 1024 pulse ttl i try run motor with feedback encoder and dc motor run, but speed unstable like use the tacho generator.. how to set parameter with encoder in simoreg ?
-------------- |
Last edited by: Min_Moderator at: 2/18/2015 3:46:51 PMNew subject after splitting |
|
2/20/2015 8:08 AM | |
Posts: 3 Rating: (0) |
i have two pulse with output A and B . Condition of motor is running but speed actual not stable.. should i optimized speed control |
2/20/2015 8:22 AM | |
Joined: 8/25/2006 Last visit: 4/18/2024 Posts: 2203 Rating: (277) |
Hello. You didn't mention the type of Simoreg. Yes, try to optimize speed control. |
2/20/2015 9:35 AM | |
Posts: 3 Rating: (0) |
sory bos..type simoreg 6ra70.. |
2/20/2015 10:21 AM | |
Joined: 8/25/2006 Last visit: 4/18/2024 Posts: 2203 Rating: (277) |
Look at parameters P140-P148. |
Follow us on