7/24/2019 10:31 AM | |
Joined: 4/28/2015 Last visit: 10/9/2023 Posts: 394 Rating: (55)
|
Hello, do you want to use the TM PosInput in combination with an encoder as axis feedback. Are you using technology object "axis" in CPU? If you do like that, you have to configure the TM PosInput for motion control usage (in hardware configuration) and afterwords you could use PLCopen function "MC_Home" to set start value of the encoder... For more information, please have a look to the manuals:
And if need some information about connecting the technology module TM PosInput, you could have a look into the following application example:
|
Follow us on