4/16/2019 11:33 AM | |
Joined: 3/14/2010 Last visit: 4/14/2024 Posts: 359 Rating: (5) |
I have the similar problem in TIA v.13 Professiоnal. I configure the TP1500 Comfort OP and try to put 2 trends (from PLC, but not from archive) with different scales in the same "Trend View". I want the left value axis to display scale for the 1-st trend and the right one - for 2-nd. In runtime the trends go from right to left. The scales for sensors : 0...150 & 0...600 and must be put on the same "Trend View". The left value axis changes it scale automatically when the tag value increases more then 150 and displays all values correctly. The right value axis displays all values incorrectly and doesn’t change its scale automatically despite it was configured like …“Range” – “Auto-size”. All trends correspondent to left value axis. I want the trends to correspondent to right value axis correctly . Is it possible at least to set up the value axises vice versa ? Is there better (or the best) way to set up 2 trends with different scales in the same "Trend View" ? See attachments. ------------------------------------------------------------------------------------------ Attachment2 trends with different scales.zip (105 Downloads) |
Last edited by: Alex3110 at: 4/16/2019 11:41:49 AMLast edited by: Alex3110 at: 4/16/2019 12:48:36 PMLast edited by: Jen_Moderator at: 4/16/2019 1:39:27 PMNew subject after splitting |
|
4/16/2019 3:08 PM | |
Joined: 7/19/2011 Last visit: 4/22/2024 Posts: 262 Rating: (5) |
Hi Alex3110 You can configure 2 Different scale in same trend view just use Left Value Axis and Right Value Asis . Same can be selected individually for different pen in Trend Window under Properties >>Trend >> Side (Left/Right). Please check attachment for reference. AttachmentTrend Scale.docx (304 Downloads) |
Last edited by: javed88 at: 4/16/2019 3:09:52 PMJAVED AKHTAR |
|
This contribution was helpful to2 thankful Users |
Follow us on