Industry Online Support
Technical Forum
7/2/2008 4:12 PM | |
Posts: 10 Rating: (0) |
I am using WinCC V6.2 SP2. I start another program.exe in parallel when WinCC starts (By adding the program in the startup list). Now how do I show this program in a picture window of WinCC while WinCC is running? There should be a C-Script with display functionalities?Could the ones mentioned in this thread (WinCC : lose of focus of external windows)be used? |
Last edited by: CS Moderator at: 7/3/2008 12:22 AMnew subject after splitting refered thread inserted |
|
7/3/2008 10:52 AM | |
Posts: 1776 Rating: (95)
|
Hi, yes it should work. also have a look at this FAQ http://support.automation.siemens.com/WW/view/en/2522765 |
Follow us on