5/27/2013 11:12 PM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating: (53) |
You can read about it here. The main subject of a Tip was some other function, though it is also clear how to use VBA and hotkeys to switch between languages. Regards |
This contribution was helpful to2 thankful Users |
5/29/2013 9:19 AM | |
Joined: 6/13/2012 Last visit: 10/19/2022 Posts: 161 Rating: (4) |
Thanks for coming to everyone!!=) Look at this @PG_VSwitch2_Parameter.PDL, please, when i try to derive texts with "TextDistributor", there is only little part of texts, in the result file. Languages are: Russian and and English. WinCC 7.0 SP3 And i have the error like "Object ref not set to an instance of an object" in the result list after making *.csv file. (unknow object and subobject)
Attachment@PG_VSwitch2_Parameter.zip (104 Downloads) |
5/31/2013 8:37 AM | |
Joined: 6/13/2012 Last visit: 10/19/2022 Posts: 161 Rating: (4) |
I use PCS 7 V8.0. There is the attachment with some pictures,how i try to export texts. As you see, the result OS_GraphicsDesigner.txt have a small part of source *.pdl
Attachmentsample.zip (106 Downloads) |
6/2/2013 1:16 PM | |
Joined: 6/13/2012 Last visit: 10/19/2022 Posts: 161 Rating: (4) |
Do you mean Update 1? There isican download (free) Update 1 only,to install it over my prev system PCS7 v8? Thanks.
|
Follow us on