3/27/2013 7:42 AM | |
Joined: 10/11/2006 Last visit: 4/24/2024 Posts: 5823 Rating: (789)
|
Dear Shank, take care, that for going to the boot mode, the pins 9,5,1 and 4 must by bridged. See also attached file for firmware update on CUMC (the cable is the same for CUVC). AttachmentREADMEMC.PDF (528 Downloads) |
Last edited by: O_Moderator at: 4/2/2013 9:16 AMWith best regards, |
|
3/27/2013 9:37 AM | |
Posts: 56 Rating: (7) |
Dear TechTeam,
Thanks for your reply I am communicating with the drive with the same cable & cable as per specification which you given.also 9,4,1 are bridged. Could you tell me one thing after connecting the cable at one end PMU & second end at PG serial port, make the power supply switch ON for the drives, the PMU will directly dispaly the status'E' orany thing? AttachmentLoading Firmware.pdf (531 Downloads) |
Follow us on