9/9/2013 9:40 PM | |
Joined: 8/31/2010 Last visit: 4/14/2024 Posts: 1509 Rating: (222) |
Hello ThaKibosh, It is very well possible to detect hardware list of S7-1200 and S7-1500 using a unspecified CPU option. Am not sure of this possibility for S7-300 and S7-400 systems. Check this out for the procedure to upload program blocks - How do you load the project data from the CPU into the programming device in STEP 7 (TIA Portal)? Online Backups are applicable only for S7-300 / S7-400, not for S7-1200 / S7-1500. Here the complete HW config + blocks are stored as binary code (the code can't be opened using TIA Portal) and also it can be restored to the S7-300 / S7-400. |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
12/13/2013 12:40 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
New question splitted to uploading S7-1200 Best regards O_Moderator |
This contribution was helpful to1 thankful Users |
3/11/2014 9:04 AM | |
Joined: 5/31/2011 Last visit: 4/24/2024 Posts: 190 Rating: (31) |
Not yet Jieve, But I've heard (not sure yet) it will be coming in version 13. |
Follow us on