8/28/2018 4:50 PM | |
Posts: 88 Rating: (4) |
How to use 4-20mA analog input to 6ES7 231-4HD32-0XB0 AI module in which this module is accepting 0-20mA. |
8/28/2018 5:15 PM | |
Joined: 9/21/2012 Last visit: 9/23/2024 Posts: 4161 Rating: (464) |
You can configure this module to use +/-10 V, +/-5 V, +/-2.5 V, or 0-20 mA/4-20 mA. So i don't see a problem here. |
8/30/2018 4:07 AM | |
Posts: 5 Rating: (2) |
I think it's not a problem.0~20mA means 0~27648 in program,so 4~20mA means 5529.6~27648. |
Follow us on