12/21/2016 1:58 PM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
On the IOT2040 there is an additional LED (H6). With this one you can change the color of the USER LED to orange or red in addition to green. To do so extract the attached .zip folder and copy the extracted python script (setledcolor.py) to your IOT2040. I copied it to /etc. Then go to the directory where you stored the script. In my case:
set execution rights to the script
execute the script with a parameter for the color
Attachmentsetledcolor.zip (847 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to2 thankful Users |
1/21/2017 1:29 PM | |
Posts: 3 Rating: (0) |
Would be great if you could provide an exampke code snipped to use both LED's in C++ Thanks |
1/23/2017 4:41 PM | |
Posts: 30 Rating: (5) |
Mr. G, you're looking for the mraa library. https://github.com/intel-iot-devkit/mraa Look at this example, should give you the general idea: https://github.com/intel-iot-devkit/mraa/blob/master/examples/c%2B%2B/initio.cpp |
1/28/2017 3:59 PM | |
Posts: 3 Rating: (0) |
Hi Epy; MRAA is well known, but how should i use the red LED with mraa? Regards |
1/30/2017 5:48 PM | |
Posts: 30 Rating: (5) |
My bad, opened up that Python file and immediately saw mraa, thought all that I/O was done through it. Good catch DevGuy. |
3/21/2017 9:07 PM | |
Posts: 439 Rating: (108) |
Hello, Found it, thanks to AutoGen_2630904. Access input pins, user button and multi-colour user LED from node-redBest regards, Hugo |
Follow us on