Industry Online Support
Technical Forum
7/21/2009 10:18 AM | |
Posts: 767 Rating: (69) |
Many thanks daga I got confused with this https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=841294&objAction=csOpen&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW Entry ID:841294 Its says 60 and also shows that I cannot use the Alarm_8P and Alarm_8 blocks with 319-3 PN/DP (a pain although this CPU is much expensive than 414-2). There is no way that I will have 60 active alarms at the same time so it means I can go for Alarm_S or Alarm_SD. Can you please confirm that that figure 60 only means 60 active alarms. |
7/21/2009 10:45 AM | |
Joined: 3/18/2009 Last visit: 2/8/2022 Posts: 306 Rating: (94) |
v2.7 and above of CPU 319 supports 300 message S blocks.That entry needs updating. And yes, it is only for simultaneously active alarms. Do remember that an "unacknowledged" alarm is consider as active. Unfortunately, they don't support Alarm_8 (and the siblings)
|
Last edited by: daga at: 7/21/2009 10:46 AM |
|
Follow us on