3/21/2012 5:43 PM | |
Posts: 1 Rating: (0) |
Hello how to use SFC14/SFC15 to read and write data to the inverter, am beginner. |
3/21/2012 6:09 PM | |
Joined: 9/27/2006 Last visit: 9/22/2024 Posts: 12282 Rating: (2684)
|
Hello Transf.; In the following FAQ you will find a sample project susing SFC15/SFC14 to read/writwe consistent data to a Siemens drive: Are there program examples for the Instruction Manual of the MICROMASTER PROFIBUS option module? But I have generally found you do not have any advantage to use consistent data on a drive ("consistent data" basically means that you are transfering large amounts of data as a single unit, in a single communication cycle). It is much easier to use standard Load/ransfer operations to control a drive, as you generally do nmot change the speed reference everyinme you send a different control command. You will also find a project using standard Load/Transer operations in the same FAQ, compare it to the one on SFC15/SFC14. Hope this helps, Dniel Chartier |
This contribution was helpful to2 thankful Users |
7/8/2013 12:44 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Follow-Up-question splitted to how to open a example programm? Best regards O_Moderator |
9/16/2013 7:55 PM |
|
Joined: 9/16/2013 Last visit: 11/12/2023 Posts: 145 Rating: (16) |
Hi, Here you are some document can help you. Good luck hag010
|
11/17/2014 11:32 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|