9/1/2008 4:50 PM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hi, Have you seen these faq's: http://support.automation.siemens.com/WW/view/en/17532609 http://support.automation.siemens.com/WW/view/en/8782948 http://support.automation.siemens.com/WW/view/en/13654633 http://support.automation.siemens.com/WW/view/en/13542666 http://support.automation.siemens.com/WW/view/en/17413251 Perhaps they are useful Best regards, Wizard |
9/3/2008 7:35 AM | |
Posts: 13 Rating: (0) |
Hi! I decided first to work STEP by STEP as described in this manual issued by Siemens http://support.automation.siemens.com/WW/view/en/17532609 Which seems quite easy. The problem is when I come to page 18 and try using the System Configurator - what I got is not quite the same as in the manual, I’m not receiving status OK of the connection, instead I have a big red FAIL mark – see the attached picture. Does some one know what is wrong? I tried pre-installing Simatic NET but it didn’t help, I’m also running SimaticNET V6.2 CD 11/2003 + SP1 could this be the problem? Thank you! |
Last edited by: O_Moderator at: 9/16/2010 3:01 PMlink edited |
|
9/18/2008 3:43 PM | |
Posts: 13 Rating: (0) |
Hallo again! I need to renew this subject, now I’m one step further, at least I think so J I didn’t go for DASDIRECT but followed this instruction from Siemens http://support.automation.siemens.com/WW/view/en/17532609to configure Simatic NET and Softnet-S7 (I’m not quite sure what is Softnet-S7 and if it’s running, but I receive an license alarm at least which makes me think it is active) Any way, now it seems that everything is running well on my Ethernet (on each side of the cable) , when I open NetPro and RUN status on both sides of Ethernet (PLC and PC) it is showing that the devices are running and S7 communication is correct configured. So long so good. But how I connect InTouch with the PLC, I couldn’t find description of that, as you know InTouch needs defined AccessName with it’s NodeName, ApplicationName and TopicName. But how do I do that ??? And I don’t find any description of the definition of the ItemNames for the tags in InTouch. Can some one give me some ideas, advices, written documents for that? Thank you! I read the manual again and a question comes …………. Can I make a communication with a standard Ethernet card on my PC (what I’m trying ) ??? do I actually need a CP card from Siemens to do all this stuff ? I tried to configure DASSIDirect once again but I failed again L it seems I have no connection between PC and PLC – can it bee the lack of special CP card the reason ? I worked as described from Wonderware TechNote 355 but translated for S400 PLC J Tell me do I need CP card for my PC or standard Ethernet card is enough ??? may be the worls is not so simple as I thought J Thank you! |
Last edited by: O_Moderator at: 9/16/2010 3:02 PMlink edited |
|
Follow us on