12/4/2020 7:08 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, In Program zip folder you find folders namely ARC, CMA, DEF, Diagnose, & WPD. In those folders 840DSL related files are provided which can be open in Wordpad. ARC folder contains arc files of winder application NC variables. CMA folder contains part program variables & file. DEF folder contains different variables like GUD, winder specific applucation variables etc. Diagnose folder contains information about data settings related with diagosis. WPD folder contains directory, part program files & setting variables. This is application specific information in addition to standard 840D SL CNC controller commissioning information. This application is executable with Sinumerik 840D SL system + Sinamics S120 drive. It is optional & user need to procure as a option along with CNC + drive system. You get more detail information about this application in 109482268_Application_winder_with_tension_control_en document. HTH |
3/8/2021 3:08 AM | |
Joined: 8/8/2020 Last visit: 4/8/2024 Posts: 7 Rating: (0) |
Hello friend, I am trying to make an application similar to this one, could you help me? |