11/3/2020 4:33 PM | |
Posts: 198 Rating: (60) |
Hello DPCS, For “I just want to design a template layout and any code ( C action ) that is triggered will cause the template layout to be filled by reporting the relevant variable.” You can consider using the Report designer in WinCC for designing templates for reports. You can refer to Chapter 10: Creating Page Layouts in the below mentioned manual for detailed explanation and steps: WinCC V7.4: Working with WinCC https://support.industry.siemens.com/cs/ww/en/view/109736220/84045767563 SSMOpenTopFieldFixedSizeis the command to use for opening up pop up windows. You can refer the below mentioned manual to further customize the script based on your requirement. An example application/syntax of the function is as follows: SSMOpenTopFieldFixedSize(SSMGetScreen("@screen"),"@Local::Popup.PDL"); The Wincc scripting manual will help you with detailed explanations regarding the functions and commands for Scripting WinCC V7.4 Scripting: VBS, ANSI-C, VBA https://support.industry.siemens.com/cs/ww/en/view/109736230 There were prior discussions in the forum related to popup windows using C-script which might be helpful for your requirement: |
Last edited by: TechnoBlaze at: 11/03/2020 16:33:57Last edited by: Jen_Moderator at: 11/04/2020 06:35:36Optimized links. |
|
Follow us on