3/19/2012 7:49 AM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242)
|
Hi,
Try to download some application from your computer to panel via this port or at least you can try to update OS. When you do so, you have the ability to check current OS on the panel, so during check you will see if computer gets connected to the panel or not.
These two questions are pretty about the same. It is good idea at least to indicate diagnostic events on alarm field in order to see what's the status of communication to PLC. What about your link is that this procedure should be supported on TP177B as well. So try to do it and see what's the status of connection. If you don't want to go throigh the procedure in the link given you can at least do what is in attached pictures in order to have overview of you connection status. AttachmentScreenHunter_06 Mar. 19 08.51.zip (188 Downloads) |
Last edited by: Darius at: 3/19/2012 7:54 AMBest regards, |
|
Follow us on