Industry Online Support
Technical Forum
12/29/2011 7:50 AM | |
Posts: 2964 Rating: (482)
|
Hello.... Standard squarewave encoders (TTL) with differential signals according to RS422 and 5 V power supply voltage can be connected as pulse encoder for induction motors to the control board "SIMODRIVE 611universal HR/HRS" (Order No. 6SN1118-NH01-0AA) The maximum encoder limiting frequency is 420 kHz. Check this document...... Regards, Prakash AttachmentConnecting induction motors with TTL encoder (from SW 8.1).pdf (251 Downloads) |
1/2/2012 7:21 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello Experts, Can anyone reply on above points? Thanks in advance. DEEP. |
Follow us on