Industry Online Support
Technical Forum
3/15/2010 10:43 AM | |
Joined: 3/26/2009 Last visit: 3/31/2024 Posts: 134 Rating: (0) |
Dear sirs. How you configured the PC and MicroWin [PG/PC] connections that would connect with the PLC in a Teleservice mode? |
Last edited by: O_Moderator at: 3/17/2010 8:25 AMLast edited by: O_Moderator at: 3/17/2010 8:24 AMnew subject after splitting from /tf/WW/en/Posts/37809#top |
|
3/15/2010 4:29 PM | |
Joined: 5/28/2008 Last visit: 4/9/2024 Posts: 1343 Rating: (141) |
Hi, I think it is the link that Lifrasil posted one entry above yours, isn't it? |
3/17/2010 8:28 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread How download project via MD720-3?. Best regards O_Moderator |
Follow us on