9/22/2008 2:40 PM | |
Posts: 38 Rating: (0) |
Hey all, I am running WinCC V5.1 and I am having the following errors appear when I try and open the project. HResult Error 0x2: System cannot find the file specified. HResult Error 0x80046206 : (null). I have checked the following link https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=23711489&caller=viewhowever, after doing what is suggested, the project still will not load. Has anyone had experience with these errors before? Any help would be appreciated. Thanks |
9/22/2008 3:10 PM | |
Joined: 9/11/2006 Last visit: 3/17/2022 Posts: 168 Rating: (6) |
Hi maybe the following link can help: http://support.automation.siemens.com/WW/view/en/6836122 |
9/22/2008 5:27 PM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
|
Follow us on