9/16/2006 2:35 PM | |
Posts: 3149 Rating: (171)
|
Hi as so often an FAQ can help - did you already check them??? http://support.automation.siemens.com/WW/view/en/6836122 nemo |
9/17/2006 11:17 AM | |
Joined: 1/17/2006 Last visit: 2/7/2022 Posts: 171 Rating: (0) |
dear nemo on client PC i am logging on through a local user ID for windows LONGON. and then i am opening WINCC explorer->open existing Project->then i am browsing the *.MCP file which is located on Server. whats next? muneeb |
9/17/2006 12:15 PM | |
Posts: 3149 Rating: (171)
|
Dear Muneeb, a) did you already check, whether your *.mcp is write-protected???? b) which user-rights do you have on the client and server (admin? power user??) c) Is this user known at your server as well?? d) can you open your project on your server without any problems? nemo |
9/17/2006 1:40 PM | |
Joined: 1/17/2006 Last visit: 2/7/2022 Posts: 171 Rating: (0) |
dear nemo 1.yes the user is local on client PC and is an administrator. 2. project is being opened on server itself without any error. Now i am making client in other way, in which i am creating a SERVER DATA on server (*.Package file). then i am adding one client PC in my Server WINCC project. then i am defining a startup screen on client PC. On Client side PC i am defining a startup screen of server, everything is running fine. Now my problem in this client is the OS-Project buttons on server side(like arrow button, Key button(to logon and logoff), Alarm control window, these are showing deactive on client Pc. what could be the reason? |
9/18/2006 1:02 PM | |
Posts: 3149 Rating: (171)
|
Hi Muneeb, did you proceed acc. to this FAQ when you tried to open your project from the client (first part of your forum-thread)?? http://support.automation.siemens.com/WW/view/en/22593197 http://support.automation.siemens.com/WW/view/en/15121778 When you started with Client/Server did you proceed as mentioned in "WinCC online help > Configuation> Client /Server"? Did you create WinCC-users with the corresponding rights on your WinCC-Client?? nemo |
9/19/2006 8:13 AM | |
Joined: 1/17/2006 Last visit: 2/7/2022 Posts: 171 Rating: (0) |
Dear Nemo The problem is still there. the Faqs which you reffered to are reflecting to what i am trying to do, but the problem is i am when i am trying to open a server project on CLient WINCC, i am not prompted for SYStem LOGIN ID and PASSWORD. Infact i am given a message as i told you earlier "Access to the project denied". i want to know why this message is appearing all the time. i tried every thing with my project. anyways if you can help me, i will be thankful to you. muneeb |
9/19/2006 9:14 AM | |
Posts: 3149 Rating: (171)
|
Hi Muneeb, as mentioned before I think, that your network-configuration on the windows part is not yet sufficient, e.g. missing user rights for access..... nemo |
10/13/2006 11:07 PM | |
Posts: 33 Rating: (5) |
I agree with Nemo, Did you change the passwords at the 2 stations? Example: If the server has a user 'administrator' and the client has one 'administrator' , both stations have to have the same password for that user. I would also have to ask, did you turn off sharing on the folder containing the WinCC project? It seems to be a Windows issue, not siemen's software. Hope this helps. |
Follow us on