Industry Online Support
Technical Forum
8/30/2014 6:21 PM | |
Posts: 5225 Rating: (1192) |
Thank you for letting us know. Please consider editing the title of this thread and putting "solved" in there. Greetings. w |
8/31/2014 9:35 AM | |
Posts: 168 Rating: (5) |
Sorry for that, I've corrected it now |
This contribution was helpful to1 thankful Users |
8/31/2014 6:18 PM | |
Posts: 5225 Rating: (1192) |
Hi huggy_d1. Profinet is not just putting Profibus on an ethernet line. The trouble is that the Profinet network has x3 modes of operation. For an explaination of sorts see [LINK]. Something that you have to remember about Ethernet TCP/IP (one of Profinet bases) is that the role of sender an receiver is in flux. There is no real fixed master as we see in Modbus RTU and Profibus. But I think this discussion is beyond what was asked in this thread. As for your descriptions.. in principle the restart re-initialised the communications and established the network in a proper way much as you are explaining. Greetings. w |
Follow us on