11/15/2016 8:28 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
Hi together, I had a strange message in Step7 5.5 S4 with HF11 When I opened the HW-Config of a project from a customer, I had two not viewable modules with the message in the picture attached. HW-Config claimed that Step7 5.5 SP5 and Step7 5.6 is needed for this two modules. As I know, the latest version is Step7 5.5 SP4 HF11. Solution for this is to install the latest Hardware Support Package. You can do this in HW-config in extras->install HW-updates. Install the HSP automatically from the internet or download the HSP manually from here: STEP 7 V5.x Hardware Support Packages (HSPs - as at 11/2016) for installing hardware updates in the Hardware Configurationregards, |
Last edited by: mopS04 at: 11/15/2016 8:32:06 AMFCK WAR! |
|
This contribution was helpful to
2 thankful Users |
Follow us on