5/18/2014 1:20 PM | |
Joined: 5/10/2013 Last visit: 10/16/2023 Posts: 11 Rating: (0) |
I do not have the panel, and I have no connected any start signal. How can I give a stop? Hi is in ready not runing.. |
5/18/2014 1:22 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Does your drive has AOP? |
5/18/2014 1:24 PM | |
Joined: 5/10/2013 Last visit: 10/16/2023 Posts: 11 Rating: (0) |
No |
5/18/2014 1:29 PM | |
Joined: 5/10/2013 Last visit: 10/16/2023 Posts: 11 Rating: (0) |
When i cut the 400V power supply, inverter is off |
5/18/2014 1:29 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Then how start (run), stop & set point is applied to drive? |
5/18/2014 3:14 PM | |
Joined: 5/10/2013 Last visit: 10/16/2023 Posts: 11 Rating: (0) |
I start inverter then i give stop ( from Starter) and still cannot change this parameters |
5/18/2014 3:47 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, And the led on the front of MM4 (green and yellow) as they are? (Flashing,fixed)
|
5/18/2014 3:58 PM | |
Joined: 5/10/2013 Last visit: 10/16/2023 Posts: 11 Rating: (0) |
The led on the front of MM4 (green and yellow) are shining. |
5/18/2014 4:12 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, r0002=? P0003=?
|
5/18/2014 4:15 PM | |
Posts: 8946 Rating: (999) |
[/Quote] |
This contribution was helpful to1 thankful Users |
5/18/2014 5:34 PM | |
Joined: 10/10/2010 Last visit: 9/14/2024 Posts: 307 Rating: (15) |
the drive should be inhibited and be in commsioning mode |
5/19/2014 8:55 AM | |
Joined: 5/10/2013 Last visit: 10/16/2023 Posts: 11 Rating: (0) |
r2=0 and p3=3 I cannot change parameters(p 2012, p2013) and r2=1 and ps=3 I cannot change parameters(p 2012, p2013). |
5/19/2014 2:10 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Just follow the steps suggested by expert Mr. Vitani. |
This contribution was helpful to1 thankful Users |
5/21/2014 11:37 AM | |
Posts: 28 Rating: (4) |
Hi just give auxilary supply to drive and then change the parameter regards aakash |
Follow us on