10/17/2014 4:52 AM | |
Joined: 10/7/2005 Last visit: 9/19/2024 Posts: 3021 Rating: (1054) |
Hello behroz ok, this is not a VIPA forum, but I still believe we can help each other, moreso since this isa DP Slave question (be it VIPA CPU DP I-Slaveor otherwise) and you are also using a Siemens CPU, solet's see what we can do: First things first, please check the following: 1.) Verify that your VIPA CPU has indeed a DP Slave port (e.g. 215-2BP02) 2.) Make sure you have the correct GSD file for your DP Slave(to be provided by the Slave manufacturer, i.e. VIPA) 3.) Make sure you have importedit into the Simatic Manager as per How do you integrate a GSD file into the STEP 7 HW Config for PROFIBUS or PROFINET? Questions: 4.) Have you already configured it? (see also DP link between CPU 315-2DP (slave) and S7-400 (master) with STEP 7 V5.3 as a general example on how to do so) 5.) If already configured,what error(s) do you have (the more details you can provide us with the better) I hope this helps |
Cheers |
|
This contribution was helpful to2 thankful Users |
Follow us on