Industry Online Support
Technical Forum
10/16/2009 7:36 PM | |
Posts: 691 Rating: (37) |
Try for PC Adapter(Auto) and go for Start "Network Detection" in the Properties Tab also check the local connection is set to USB instead of COM... |
10/19/2009 3:29 PM | |
Joined: 5/28/2008 Last visit: 9/11/2024 Posts: 1343 Rating: (141) |
If this doesn't help, switch PLC in STOP and then try again download. |
11/6/2009 3:50 PM | |
Posts: 62 Rating: (0) |
Hi, Also Double check to make sure that you have the swcith on the PLC in (Term) position. Regards, Raymond. |