9/23/2010 11:50 AM | |
Posts: 14 Rating: (0) |
Hi again! I'm back again with my doubts, hopping you'll help me again as good as you made before. Thanks everybody. Right now, I achieved to conect and configure both SCALANCE w788 and 744 and I've connected them but there are not working. I've got the master connected to an switch, and the 788 acces point to the switch too and in the other part the W744 with the slave. I've configured the W7XX to work in 2.4 GH 58 Mbps and they have key sequrity. nothing special. But I really don't know If I have to do something more, I've read a tutorial about all this and it is supposed to work after the configuration, but it doesn't. Any clues why this happens¿ if you need more information I'll give you. Thanks for your help! Splitted from x208. |
Last edited by: O_Moderator at: 9/24/2010 9:41 AMnew subject after splitting |
|
9/29/2010 5:58 PM | |
Posts: 14 Rating: (0) |
I don't know where exactly the failure is at. I do have 1 IO device only after the 744 whose update time is 16ms 3 times. I already had got the adopt MAC manually and there written the ET200 MAC address. so... where could be the problem at? here youve got the files I taked from the w788 and w744 of the configuration, I guess I made it correctly.I hope you can find a solution in there. thanks! Attachmentconfiguration.zip (203 Downloads) |
Follow us on