1/15/2013 8:06 PM | |||||
Joined: 12/24/2012 Last visit: 5/18/2023 Posts: 26 Rating: (0) |
This programming package is just for Step 7 V5.4 SP5?, in Step 7 V11 exist some package like this? i also checked in the hardware catalog of Step 7 V5.4 SP5 and it doesn't appear, i upgraded and nothing. Thanks |
||||
Last edited by: Roxitaa at: 1/15/2013 11:17 PM |
|||||
1/15/2013 8:24 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, Maybe this helps : Regards, Marcjan |
Problem solved? |
|
1/16/2013 8:08 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
You need to install aditional software package which is mentioned in my post before. It is not Step7 only. And Technology CPU is not available yet in TIA portal. Best regards, Hristo Mihalev
|
This contribution was helpful to2 thankful Users |
1/16/2013 5:47 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328)
|
You need STEP 7 V5.5 and S7-Technology to be able to program this CPU. (After you installed it, you have to select the "S7-Technology" profile in HW Config) If you want to use the Safety functions of this CPU,you need additional SIMATIC Distributed Safety. See Chapter 2.4 for theS7-Technology manual for more details. |
|
|
This contribution was helpful to1 thankful Users |
Follow us on