12/22/2007 6:06 PM | |||||||||||||||
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Hi Ghost, If you want to know more to build up a Profibus network then the next handbook will help: SIMATIC NET PROFIBUS Networks Aret mentioned that he never goes to a higher Baurate then 187,5 kBit/s..... on this length of network. With 187,5 kBit/s you may go to 1 km.... So the next step 500 kBit/s is (for sure) useable for 400 meter. If you built up the network as mentioned in the handbook and use the right cablework and the right connectors, like the Profibus Fast Connect connectors, then you may go even to 12 MBit/s with the length you have ...... The connectors that are perfect are:
|
||||||||||||||
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|||||||||||||||
Follow us on