4/26/2019 6:34 PM | |
Joined: 5/31/2016 Last visit: 8/9/2022 Posts: 20 Rating: (0) |
Hello everyone, I have a TP177B Mono DP Hmi, while Transfer project I get "insufficient Storage error". As mentioned here I want to restore Panel, according to I read " It is not possible to load and edit a backup file in ProTool or WinCC flexible. The file can only be reloaded to the original or another panel via a restore with ProSave." So I need a another panel .psb file to restore mine. Is there someone to upload it to me ? Best Regards. |
4/28/2019 2:24 PM | |
Joined: 5/31/2016 Last visit: 8/9/2022 Posts: 20 Rating: (0) |
I solved problem with changing download path in transfer settings. It should be "\Flash\Simatic\" |
Follow us on