Industry Online Support
Technical Forum
3/11/2008 1:12 PM | |
Joined: 1/17/2007 Last visit: 10/6/2020 Posts: 289 Rating: (3) |
Dear Danielle, Can you explain in detail this ? /tf/WW/en/Posts/16390 "hi ionut.b, your idea to replicate the external wincc tags with wincc option redundancy is very good, but it is not possible!!!!!!! WinCC (since WinCC V6.2)provides the opportunityto replicate internal wincc tags of two redundant servers only. For this reason youwill find for each internal tag the check box "Tag synchronization" in dialog "tag properties". For external tags the check box "Tag synchronization" is disabled." I have a redundant system (2XCPU414H-4), and I need to monitor it form two separate PC (WinCC RT). The compete system shold offer redundancy as: - one of the PLC fails (done with H system); - one of the FO paths fails (the comm path ethernet it cabled twice); - one of the PC fails (I should be able to see the proces from the other PC). From the WinCC point of view I have the following questions: - since I will only have two PC (client not server) with WinCC RC+RT, can I sync continously the two PC with WinCC Redundancy? As ateam mentioned in his post can I use WinCC Redundancy for this (process and internal tags) ? Only one license of WinCC Redundancy is enough fot my application? Where to find all the detailes about WinCC Redundancy (delivery pack contents) ? Thank you very much. |
Last edited by: CS Moderator at: 3/25/2008 12:38 PMnew subject after splitting |
|
3/11/2008 5:23 PM | |
Posts: 1275 Rating: (123)
|
Hi ionut.b, I'll reply to your other thread, so the subjects won't be mixed up, ok? So you'll find my answer on this link. Best regards, Danielle |
3/25/2008 12:40 PM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
closed cause question posted twice. The second thread with the subject Network Configuration Redundand System with PLCs and WinCCis published within the conference Communication / Networks. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on