Industry Online Support
Technical Forum
2/17/2010 4:42 PM | |
Joined: 4/21/2009 Last visit: 3/4/2024 Posts: 38 Rating: (0) |
Hello, I have tried using SFC36 and it appears to execute without errors, but Istill get errors in thediagnostic buffer and requestsOB122 (as shown in the diag buffer). SFC12 is also not included as part of my current firmware, so this is not an option for me either. Am I doing something wrong, or is there another way? I am doing significant bench testing with the non-IO programming logic. Disabling these types of errors would allow me decipher my program errors better, as right now the IO Access Errors fill the dia. buffer. Thanks in advance |
Last edited by: O_Moderator at: 3/1/2010 9:21 PMnew subject after splitting from /tf/WW/en/Posts/38987#top |
|