Industry Online Support
Technical Forum
5/5/2014 2:35 PM | |
Posts: 220 Rating: (11) |
Hi, I hopethis FAQhelps.
|
5/5/2014 4:40 PM | |
Posts: 567 Rating: (107) |
Hi, the differnence between AS PO and AS RT PO is that AS POs are use for scaling the performance of the CPU 410-5H. If you use another S7 4xx CPU you don't need AS POs. Information about the scaling of the CPU by using system expansion card with ASPOsyou can find under the following Link (Chapter 2.10 "Scaling and licensing"). Information about the AS RT POs you can find under the recommended FAQ by "No Name". |
Follow us on