1/17/2013 3:33 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, The reason for stopping the CPU can be found in the diagnostic buffer. the corresponding error OB's can be found there too. So have a look at that information. It could well be thast one off the RIO is going down when power is lost, if not the right error OB's are in the CPU that will cause the stop. See also: Which organization blocks do you need for error handling? Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
Follow us on