1/28/2018 10:58 AM | |
Posts: 8 Rating: (0) |
Posting to my colleagues ...... if anyone can help me and advise me. It's the Atlascopco GA50VSDff compressor in which the Simens Simovert converter ... When I start the compressor on the panel, the F027 error is displayed. There is no phase 2 .. .. I encountered a problem in the converter itself, that one IGBT changed the value of BSM300GA120DN2SE3256 ... I replaced all 6 IGBT ... after the start of the compressor is still the same error F027, I examined a driver board with no visible damage, and the elements themselves on the board are correct ... when I press the button on the converter panel itself, I get the initials P108 A017 F027 in the converter itself I have CUVC 6SE7090-0XX84-0AB0 engine 1LA5207-4AA91-ZT17 Can I get the parameters of the converter itself and manually enter it ... I have the Siemens USB to RS485 6SE7 972-0CB20-0XA0 adapter ... I have 26 years of experience in electronics, but my experience as a service technician is based on the hardware part , with the sofver I have a problem ..... thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/29/2018 1:47:51 PMNew subject after splitting |
|
2/4/2018 7:59 PM | |
Posts: 8 Rating: (0) |
Thank you for answer my friend....but i dont know what is ABB sensor? |
Follow us on