Industry Online Support
Technical Forum
3/11/2013 6:01 AM | |
Posts: 39 Rating: (0) |
Hello Experts, In one of my project, I happen to use interface module - IM - 460 - 3 (6ES7 460-3AA01-0AB0) - 1 no and IM - 461 - 3 (6ES7 461-3AA01-0AA0) - 3 nos, I have connected them as shown in the attached picture. I also have used IM461 terminator (6ES7 461-3AA00-7AA0) one no and I have connected in one end of IM 461. I have 2 doubts, firstly, Should I have to use two terminators or one is enough. and secondly, whether the architecture is OK and will work? or should I have to make any changes. Please share you views Thanks in advance Regards, Ujwal Sadare
AttachmentArchitecture1.pdf (195 Downloads) |
3/11/2013 6:29 AM | |
Posts: 1064 Rating: (72) |
Yes this will work and you do need 2 terminating resistors always |
3/11/2013 10:13 AM | |
Posts: 39 Rating: (0) |
Thank you very much Playerslight for you immediate reply.. I will consider two terminators |
Follow us on