4/23/2010 11:12 AM | |
Posts: 3 Rating: (0) |
Hi Two Questionss: 1) For CBA for creating PROFINET component. Under "Storage Areas" tab, the "Target library", and "Target Library and file system" is greyed out. Also how to make the connections between the componets when they are created. I am using Step 7.V5.4+SP5, and Imap add on V3.0+SP5. The manuals seem to explain use of imap as a separate package, and not much information on the step 7 add-on. second question is splitted to Can port mirroring be used on IM151-8. |
Last edited by: O_Moderator at: 4/26/2010 1:20 PMnew subject after splitting second question to new thread |
|
4/23/2010 3:45 PM | |
Posts: 5822 Rating: (411)
|
Hello,
|
Last edited by: O_Moderator at: 4/26/2010 1:21 PM |
|
Follow us on