Industry Online Support
Technical Forum
3/20/2008 7:54 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello Rollingclone; To setup PA slaves on a DP/PA link, you have to create a single gsd file that will include all the PA instruments on that link (no matter how many couplers are on the same link). Siemens provides a tool for that: gsdtool. You can find it on the following link, along with instructions: http://support.automation.siemens.com/WW/view/en/26562190 Note that for gsdtool to work, you need to install the latest java compiler for your version of Windows (see the instructions in the link provided), Also note the limitations that a single DP slave must adhere to, number of input data, output data and parameter data. If you exceed any of them, the gsdtool will warn you and stop the process. Once you have created the new gsd file for your PA application using gsdtool, install it in ypour Profibus configurator as you would any new gsd file, and use it to insert a DP/PA link in your configuration. Hope this helps, Daniel Chartier |
Follow us on