Industry Online Support
Technical Forum
11/10/2009 7:55 AM | |
Posts: 37 Rating: (2) |
Hi All,
I am facing a problem with configuring the IM 153-2 with S7 315 that I cannot compile the IM153 in the hardware configuration and gives the error number: (1230:3000). At the same time I was testing this IM153-2 with other project (S7 313) that was fine and no error!! You can see the hardwire configuration for both project attached. So I do not know?? is there a compatibility issue or I need to do a further step!Any help would be appreciated. PLC Product #: 6ES7315-2EH13-0AB0. IM153 Product#:6ES7153-2BA02-0XB0 Thanks Mans AttachmentIM153-2.zip (222 Downloads) |
Last edited by: MANS at: 11/10/2009 9:45 AMLast edited by: MANS at: 11/10/2009 9:44 AM |
|
11/10/2009 12:20 PM | |
Joined: 8/25/2005 Last visit: 7/5/2024 Posts: 1161 Rating: (110) |
Hello MANS, could you please publish the information given behind the button Details Best regards Sabine |
11/10/2009 4:27 PM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Dear MANS, I have did the HW config as per your attached pictures without errors in compilation. Really I do not know what's the reason of this error in your configuration. In any case, here's attached an archive of the project I have made for you. Open HW config and check it. Regards, Attachment315_2pn_.zip (246 Downloads) |
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
11/11/2009 8:50 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello Mans, Glad to hear you already solved problem. I want just tosay afew "words". IM153-2 (6ES7 153-2BA02-0XB0) require STEP7 V5.4, SP3 - so you have it. I don't think this wasthe problem. But you said "I received error message 1230:3000 .
If we take this like starting point and look at Consistency error after configuration of the CPU as time slaveperhaps this could be real reasons for your "troubles". With regards, Hristo Mihalev |
Follow us on