9/2/2021 10:03 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936)
|
Hi, Take a look at the Industry Library (Link), it features two additional valves: VlvDsL and VlvDiv (see attachment). The VlvDsL is a double seated valve and is drawn as a four way valve. However, the block only features open and close and open/close top and bottom seat. Another option is the VlvDiv which is a diverter valve that can be set to 8 positions max. Maybe one of these block is useful to you? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on