2/1/2019 6:40 AM | |
Posts: 2 Rating: (0) |
Hey guys New here and would love some of your support. Here is my issue. So far I have located an old project entitle: OPC Client Excel Applications for Data Access to PCS 7 OS Process Data via OpenPCS 7 So I am planning to use how they connected to the OPC server in my project. I discovered that they used a DLL called sopcdaauto.dll which seems to store all the functions they used in that project so I am going to try and porting the vb scripts to c# .net. So far I was able to make reference to the DLL and be able to view the classes in the object browsers on both vba and Visual Studio. So I am starting with porting this code from the vba:
Here is the code that i tried
And the system makes me build the code myself. Unfortunately, I am not sure how the code for the function works as I can't seem to open it. Can you someone help me, please? or tell me if I imported the DLL correctly or missing anything to use it? |
Last edited by: Anthony21893 at: 2/1/2019 6:56:41 AMLast edited by: Jen_Moderator at: 2/1/2019 12:01:26 PMOptimized link. |
|
Follow us on