4/3/2014 12:40 PM | |
Joined: 3/19/2010 Last visit: 4/17/2024 Posts: 438 Rating: (12) |
Hello, I have read all the topics about beginner steps for AS-OS engineering, in order to import tags from Step7 project to WinCC v7.2 app. But for some reason, after Compile OS procedure I am not getting any tag from Step7 symbol list in my WinCC. I have created one very simple configuration for testing, with one CPU314, with 2 I, 2IW, 2Q, 2QW variables, and I also created two DB-s with some integer values inside. Saved, compiled, everything by the book...and it doesn't work! I dont get tags in WinCC! What did I miss? My project is attached. What other option do I have when I want to import especially a lot of DB-s in my project, even when it is not integrated? Unfortuanatelly, I didn't find approriate FAQ for this, eventhough this is one very frequent and important question. AttachmentTestasos.zip (153 Downloads) |
4/4/2014 12:22 PM | |
Joined: 9/14/2012 Last visit: 8/22/2024 Posts: 87 Rating: (14) |
Hibanconi, Check your SystemAS-OS Engineering is installed or not, are you able to compile your Project? Any error message?? At the time of installation are you install all the files without any error. Give me more detail… |
Regards, |
|
This contribution was helpful to1 thankful Users |
4/4/2014 12:54 PM | |
Joined: 3/19/2010 Last visit: 4/17/2024 Posts: 438 Rating: (12) |
Hello Vijay, Yes, I do have AS-Os installed. Yes, I can compile the project, but I keep getting some error messages. I am sending the log file in the attachment. Installation was OK. Can you check the project I sent previously, if you can get the tags imported? Edit: Now, I deleted the DB1 which caused the problem. Now, I don't get any error during compilign, but I still can't get I, IW, Q and QW tags? AttachmentTRANSFER.zip (171 Downloads) |
Last edited by: banconi at: 4/4/2014 1:04 PM |
|
4/30/2014 9:25 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (41)
|
Hi, do you have chose the right connection inside the compile dialog? Best Regards, Healthcheck |
Grundkurs/Systemkurs WinCC V7: |
|
7/25/2014 10:08 PM | |
Joined: 9/12/2012 Last visit: 5/14/2024 Posts: 9 Rating: (0) |
banconi, you solved this problem? I also bug 15124
|
7/27/2014 10:41 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Hello, Same problem discussed in the following thread with some proposed solutions: OS Compilation error in PCS 7
I suggest reading the whole discussion and update here, Best regards, Hamid Hosseini |
Follow us on